In https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/boot/dts/freescale/imx8mp-evk.dts
&uart1 { /* BT */
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart1>;
assigned-clocks = <&clk IMX8MP_CLK_UART1>;
assigned-clock-parents = <&clk IMX8MP_SYS_PLL1_80M>;
uart-has-rtscts;
status = "okay";
bluetooth {
compatible = "nxp,88w8997-bt";
};
};
&uart3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart3>;
assigned-clocks = <&clk IMX8MP_CLK_UART3>;
assigned-clock-parents = <&clk IMX8MP_SYS_PLL1_80M>;
uart-has-rtscts;
status = "okay";
};
In https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/arch/arm64/boot/dts/freescale/imx8mp-venice-gw74...
/* GPS / off-board header */
&uart1 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart1>;
status = "okay";
};
/* bluetooth HCI */
&uart3 {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_uart3>, <&pinctrl_uart3_gpio>;
cts-gpios = <&gpio3 21 GPIO_ACTIVE_LOW>;
rts-gpios = <&gpio3 22 GPIO_ACTIVE_LOW>;
status = "okay";
bluetooth {
compatible = "brcm,bcm4330-bt";
shutdown-gpios = <&gpio3 8 GPIO_ACTIVE_HIGH>;
};
};
Two questions:
1. are propertys assigned-clocks & assigned-clock-parents necessary? What would happen if it's lacking?
2. What are the differences between the two hardware flow control methods uart-has-rtscts and uart-has-rtscts &cts-gpios&rts-gpios?
已解决! 转到解答。
Q1:
1. are propertys assigned-clocks & assigned-clock-parents necessary? What would happen if it's lacking?
A:Yes, necessary. These properties are part of the Common Clock Framework in Linux device trees. They are used to configure the clock source and parent for a peripheral at boot time.
If lacking, Incorrect baud rate if the default clock frequency doesn’t match what the driver expects.Potential instability if the clock source is not optimal for low-power or performance modes.
2. What are the differences between the two hardware flow control methods uart-has-rtscts and uart-has-rtscts &cts-gpios&rts-gpios?
A:uart-has-rtscts 是一个 Device Tree 属性,用于告诉 Linux UART 驱动该串口支持 硬件流控 (RTS/CTS),并且应该启用它。RTS (Request To Send) 和 CTS (Clear To Send) 信号由 UART 控制器硬件自动处理,不需要软件干预
The driver will enable hardware flow control( (RTS/CTS)) function when initializing UART.
cts-gpios 和 rts-gpios 是 Device Tree 属性,用于在硬件没有原生 RTS/CTS 引脚,或者需要通过 GPIO 来模拟流控时使用。驱动会通过 GPIO 来实现流控,而不是使用 UART 控制器的硬件 RTS/CTS.
Q1:
1. are propertys assigned-clocks & assigned-clock-parents necessary? What would happen if it's lacking?
A:Yes, necessary. These properties are part of the Common Clock Framework in Linux device trees. They are used to configure the clock source and parent for a peripheral at boot time.
If lacking, Incorrect baud rate if the default clock frequency doesn’t match what the driver expects.Potential instability if the clock source is not optimal for low-power or performance modes.
2. What are the differences between the two hardware flow control methods uart-has-rtscts and uart-has-rtscts &cts-gpios&rts-gpios?
A:uart-has-rtscts 是一个 Device Tree 属性,用于告诉 Linux UART 驱动该串口支持 硬件流控 (RTS/CTS),并且应该启用它。RTS (Request To Send) 和 CTS (Clear To Send) 信号由 UART 控制器硬件自动处理,不需要软件干预
The driver will enable hardware flow control( (RTS/CTS)) function when initializing UART.
cts-gpios 和 rts-gpios 是 Device Tree 属性,用于在硬件没有原生 RTS/CTS 引脚,或者需要通过 GPIO 来模拟流控时使用。驱动会通过 GPIO 来实现流控,而不是使用 UART 控制器的硬件 RTS/CTS.
There's a very serious mistake in your answer.
if:
required:
- uart-has-rtscts
then:
properties:
cts-gpios: false
rts-gpios: false
cts-gpios:
maxItems: 1
description:
Must contain a GPIO specifier, referring to the GPIO pin to be used as
the UART's CTS line.
rts-gpios:
maxItems: 1
description:
Must contain a GPIO specifier, referring to the GPIO pin to be used as
the UART's RTS line.
uart-has-rtscts:
$ref: /schemas/types.yaml#/definitions/flag
description:
The presence of this property indicates that the UART has dedicated lines
for RTS/CTS hardware flow control, and that they are available for use
(wired and enabled by pinmux configuration). This depends on both the
UART hardware and the board wiring.
if:
required:
- uart-has-rtscts
then:
properties:
cts-gpios: false
rts-gpios: false