processing limit of CAAM hardware?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

processing limit of CAAM hardware?

917 次查看
gbiradar
Contributor IV

Hi Guys,

              i'm cryptodev engine to encrypt data so i want to know what is the maximum amount of data size can caam process. say i want to encrypt streaming data of high definition video.

thanks

Ganesh

0 项奖励
回复
1 回复

774 次查看
bpe
NXP Employee
NXP Employee

This question is a bit vague. There is no global limit to the data

amount processed by CAAM. With a single descriptor, however, the

number of bytes that can be processed is limited by the size of the

LENGTH field of FIFO LOAD/FIFO STORE command, which is 16 bits. Some cipher modes,

namely counter-based, require a re-key after certain amount of processed

data to stay secure. This is, however, not a CAAM limitation.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复