processing limit of CAAM hardware?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

processing limit of CAAM hardware?

912 Views
gbiradar
Contributor IV

Hi Guys,

              i'm cryptodev engine to encrypt data so i want to know what is the maximum amount of data size can caam process. say i want to encrypt streaming data of high definition video.

thanks

Ganesh

0 Kudos
Reply
1 Reply

769 Views
bpe
NXP Employee
NXP Employee

This question is a bit vague. There is no global limit to the data

amount processed by CAAM. With a single descriptor, however, the

number of bytes that can be processed is limited by the size of the

LENGTH field of FIFO LOAD/FIFO STORE command, which is 16 bits. Some cipher modes,

namely counter-based, require a re-key after certain amount of processed

data to stay secure. This is, however, not a CAAM limitation.


Have a great day,
Platon

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply