picopi8m-revb1-sch PinMap?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

picopi8m-revb1-sch PinMap?

Jump to solution
2,343 Views
xiongding
Contributor I

Doc name is picopi8m-revb1-sch.pdf:

Which chip pin is the corresponding GPIO_P26_3V3?

is port 1 pin 26 ? 

GPIO_P44_3V3 --> port 2 pin 12 ? 

My guess:

·port 2 == (44 / 32) + 1

·pin 12 == (44 - 32 * 1)

What is the correspondence between GPIO_P** and imx8m chip pin?

微信截图_20191224124414.jpg

1 Solution
2,312 Views
igorpadykov
NXP Employee
NXP Employee

Hi xiong

for i.MX8M pins usage one can refer to Datsheet and Reference Manual (IOMUX Chapter) found on link

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
2,313 Views
igorpadykov
NXP Employee
NXP Employee

Hi xiong

for i.MX8M pins usage one can refer to Datsheet and Reference Manual (IOMUX Chapter) found on link

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------