picopi8m-revb1-sch PinMap?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

picopi8m-revb1-sch PinMap?

跳至解决方案
2,354 次查看
xiongding
Contributor I

Doc name is picopi8m-revb1-sch.pdf:

Which chip pin is the corresponding GPIO_P26_3V3?

is port 1 pin 26 ? 

GPIO_P44_3V3 --> port 2 pin 12 ? 

My guess:

·port 2 == (44 / 32) + 1

·pin 12 == (44 - 32 * 1)

What is the correspondence between GPIO_P** and imx8m chip pin?

微信截图_20191224124414.jpg

1 解答
2,323 次查看
igorpadykov
NXP Employee
NXP Employee

Hi xiong

for i.MX8M pins usage one can refer to Datsheet and Reference Manual (IOMUX Chapter) found on link

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

1 回复
2,324 次查看
igorpadykov
NXP Employee
NXP Employee

Hi xiong

for i.MX8M pins usage one can refer to Datsheet and Reference Manual (IOMUX Chapter) found on link

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------