picopi8m-revb1-sch PinMap?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

picopi8m-revb1-sch PinMap?

ソリューションへジャンプ
2,348件の閲覧回数
xiongding
Contributor I

Doc name is picopi8m-revb1-sch.pdf:

Which chip pin is the corresponding GPIO_P26_3V3?

is port 1 pin 26 ? 

GPIO_P44_3V3 --> port 2 pin 12 ? 

My guess:

·port 2 == (44 / 32) + 1

·pin 12 == (44 - 32 * 1)

What is the correspondence between GPIO_P** and imx8m chip pin?

微信截图_20191224124414.jpg

1 解決策
2,317件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xiong

for i.MX8M pins usage one can refer to Datsheet and Reference Manual (IOMUX Chapter) found on link

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
2,318件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi xiong

for i.MX8M pins usage one can refer to Datsheet and Reference Manual (IOMUX Chapter) found on link

i.MX 8M Applications Processor | Arm® Cortex®-A53, Cortex-M4 | 4K display resolution | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------