operating range for the MIPI CSI-2 camera

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

operating range for the MIPI CSI-2 camera

4,081 Views
ashokp
Contributor I

Is there any operating range for the MIPI CSI-2 camera (minimum/maximum) for receiving the MIPI data from the camera sensor?

Which clock frequency (MHz) does the below information refers to?

Reference:

As per the IMX datasheet, the following information is provided in the IPU section

Fast serial interface (MIPI-CSI2):

  • IPU receives 2 components per cycle from the MIPI-CSI2 interface
  • The maximum speed of the interface is:
  • 200Mhz for 4 data lanes configuration
  • 250Mhz for 2 data lanes configuration

The maximum bandwidth of the interface is as follows:

  • 200Mhz for 4 data lanes configuration (800Mbps/lane, 400MByte/sec)
  • 187.5Mhz for 3 data lanes configuration (1000Mbps/lane, 375MByte/sec)
  • 125Mhz for 2 data lanes configuration (1000Mbps/lane, 250MByte/sec )
  • 62.5Mhz for 1 data lane configuration (1000Mbps/lane, 125Mbyte/sec)
0 Kudos
Reply
1 Reply

2,407 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ashok

operating range for the MIPI CSI-2 is only datasheet NVCC_MIPI parameter

in Table 6. Operating Ranges

http://cache.freescale.com/files/32bit/doc/data_sheet/IMX6DQCEC.pdf

frequency refers to maximum speed of the IPU interface when receives data from MIPI.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply