netx_duo_iperf example fails to run

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

netx_duo_iperf example fails to run

1,030 Views
GLantzTCore
Contributor III

I am attempting to run the netx_duo_iperf azure example.  When I select the option to "run to main" the system hangs somewhere.  When I deselect the option, the code starts at a label named Reset_Handler.  I can step through the code until the instruction CPSIE I is executed.  Then the CPU is out to lunch.  Any suggestions?

0 Kudos
Reply
3 Replies

995 Views
GLantzTCore
Contributor III

 Thanks.  I am using the 1170 Dev kit.  I am able to run many other example programs with the i-jet probe.

0 Kudos
Reply

1,029 Views
GLantzTCore
Contributor III

I should note that I am using an IAR i-jet debug probe.  I have been using it as I test/run other examples and everything works fine.  I ran the netx_duo_ping example without issue.

0 Kudos
Reply

998 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello, If I try segger lauterbach the issue is not present, I guess this may be your board or your probe.

Regards

0 Kudos
Reply