I am attempting to run the netx_duo_iperf azure example. When I select the option to "run to main" the system hangs somewhere. When I deselect the option, the code starts at a label named Reset_Handler. I can step through the code until the instruction CPSIE I is executed. Then the CPU is out to lunch. Any suggestions?
Thanks. I am using the 1170 Dev kit. I am able to run many other example programs with the i-jet probe.
I should note that I am using an IAR i-jet debug probe. I have been using it as I test/run other examples and everything works fine. I ran the netx_duo_ping example without issue.
Hello, If I try segger lauterbach the issue is not present, I guess this may be your board or your probe.
Regards