mkfs.ext4 hangs on trying to format a file system in an encrypted partition

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

mkfs.ext4 hangs on trying to format a file system in an encrypted partition

3,207 次查看
srinidhih
Contributor I

Hello,
I'm trying to format a file system in an encrypted partition and my mkfs.ext4 command is stuck forever now.
I came across one of the old posts which suggested to reset the "CONFIG_CRYPTO_DEV_FSL_CAAM_CRYPTO_API" config, (https://community.nxp.com/t5/i-MX-Processors/Hardware-accelerated-disk-encryption/m-p/281945) I did so and it did not help resolve my issue.

As the system gets hung on the above mentioned command I'll have to reset the board to recover it. Any suggestion in this regard is appreciated.


Output after executing the command:

root@aa:~# mkfs.ext4 /dev/mapper/00000000-0000-0000-0000-000000000000-etc
mke2fs 1.45.4 (23-Sep-2019)
Creating filesystem with 65536 1k blocks and 16384 inodes
Filesystem UUID: 1e81c1cc-6f86-4a34-ad45-e3bb1cd1dd3c
Superblock backups stored on blocks:
8193, 24577, 40961, 57345

Allocating group tables: done

Details:
Yocto branch- dunfell
Board - colibri-imx6ull

Thanks
Srinidhi

标签 (2)
0 项奖励
回复
4 回复数

3,158 次查看
srinidhih
Contributor I

Hello Yuri,
I followed the documentation and enabled the necessary kernel configs and installed the suggested tools. I am  still  facing the same problem.

Some of the outputs from my system are below. 


root@trustx-cml:~# dmsetup targets
integrity v1.3.0
verity v1.5.0
multipath v1.13.0
crypt v1.19.0
striped v1.6.0
linear v1.4.0
error v1.5.0

dmsetup table --showkey 00000000-0000-0000-0000-000000000000-etc
0 2097152 crypt capi:authenc(hmac(sha256),xts(aes))-random 00000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000000 0 254:0 0 1 int
egrity:32:aead
0 项奖励
回复

3,142 次查看
Yuri
NXP Employee
NXP Employee

@srinidhih 
Hello,

  I've sent You considerations (using e-mail) regarding software approach
for cryptofs -without CAAM support.

Regards,
Yuri.

0 项奖励
回复

3,194 次查看
Yuri
NXP Employee
NXP Employee

@srinidhih 
Hello,

   You mentioned about colibri-imx6ull board. IMX 6ULL does not have CAAM;
hardware acceleration is not supported.

Regards,
Yuri.

0 项奖励
回复

3,198 次查看
Yuri
NXP Employee
NXP Employee

@srinidhih 
Hello,

   please use section  10.5 (Disk encryption acceleration) of "i.MX_Linux_Users_Guide.pdf".

https://www.nxp.com/docs/en/user-guide/IMX_LINUX_USERS_GUIDE.pdf

 

Regards,
Yuri.

0 项奖励
回复