linux kernel without network on sabrelite

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

linux kernel without network on sabrelite

1,258 Views
pratikpawar
Contributor II

Hi Community,

       I am using sabrelite board(imx6q). I am using yocto to build kernel & file system for it. I want to build a kernel without any network support(i.e. without ethernet, bluetooth, tcp/ip stack). I have disable network options in kernel menuconfig. But I got some errors while building kernel. I have attach kernel defconfig if it.

the errors I am getting are.

  LD  init/built-in.o
  LD  .tmp_vmlinux1

arch/arm/mach-mx6/built-in.o: In function `fec_phy_init':

:(.text+0xfa0c): undefined reference to `mdiobus_write'

:(.text+0xfa20): undefined reference to `mdiobus_write'

:(.text+0xfa34): undefined reference to `mdiobus_write'

:(.text+0xfa48): undefined reference to `mdiobus_write'

:(.text+0xfa5c): undefined reference to `mdiobus_write'

arch/arm/mach-mx6/built-in.o::(.text+0xfa70): more undefined references to `mdiobus_write' follow

make: *** [.tmp_vmlinux1] Error 1

ERROR: oe_runmake failed

WARNING: exit code 1 from a shell command.

 

 

thanks,

Pratik

Original Attachment has been moved to: defconfig.zip

0 Replies