Is it possible to use a single 4.3 build to support Atheros and Intel Wifi PCI-e cards

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use a single 4.3 build to support Atheros and Intel Wifi PCI-e cards

833件の閲覧回数
michaelrobbelot
Contributor IV

All,

I was wondering if it was possible, despite the differences in drivers and wpa supplicants, to support both Atheros and Intel based Wifi PCI-e cards with a single 4.3 based build. In some cases, the cards also have Bluetooth support. Thanks.

Michael Robbeloth

ラベル(2)
0 件の賞賛
返信
1 返信

727件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

I do not find any problems to have an Android Image with both drivers install to support both Wifi PCIe cards since only one of the cards it is going to be functional at time.   It is just like having a PC with both drivers and changing from one Wifi card to another.