Using the GC320 to adjust brightness, contrast, and hue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Using the GC320 to adjust brightness, contrast, and hue

ソリューションへジャンプ
4,474件の閲覧回数
sheldonrucker
Contributor III

Hello All,

I'm trying to find a way to adjust the brightness, contrast, and hue of a texture using the GC320 graphic processor on the i.MX6.   Does anyone know if this is possible?  If it is possible could you explain how or give a little example?

I've been reading through the "i.MX 6 2D API" but haven't come upon a solution.

Also, could someone point me at some example code for the 2D GPU API?  I've looked in both LTIB and the Freescale documentation but haven't found anything.

Thank you,

Sheldon

1 解決策
3,734件の閲覧回数
andre_silva
NXP Employee
NXP Employee

We Don´t have functions like that in the API, instead you could do that using the shaders (OpenGLES) or OpenCL, in this case, using gc2000.

regards,

Andre

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
3,735件の閲覧回数
andre_silva
NXP Employee
NXP Employee

We Don´t have functions like that in the API, instead you could do that using the shaders (OpenGLES) or OpenCL, in this case, using gc2000.

regards,

Andre

0 件の賞賛
返信
3,734件の閲覧回数
sheldonrucker
Contributor III

Thanks you for checking on that Andre!

Unfortunately for the application I'm working on we need to use the 2D GPU.  We've been able to get around the problem by making the color space adjustments by setting the color space conversion matrix via a frame buffer ioctl.  This has the limitation in that it effects all items drawn to that particular frame buffer.  However, we're only drawing the items whose color space we need adjusted to one frame buffer and overlaying the rest in another so that does the trick.

By the way do you know if Freescale provides any sample code for the 2D API?  If so, would you please provide me a link?

Thank you,

Sheldon

3,734件の閲覧回数
shanxigjz
Contributor II

Hi Sheldon,

I am trying to use CSC to adjust contrast of UI, do you have get this work?

could you give me some ideads how to get this work?

thank you very much.

0 件の賞賛
返信
3,734件の閲覧回数
sheldonrucker
Contributor III

Hello Gao,

I couldn't get it to work.  I ended up modifying the CSC (color space conversion) matrix in the kernel.  The only drawback with this method is that it modifies everything in the associated frame buffer.

Thank you,

Sheldon

0 件の賞賛
返信
3,734件の閲覧回数
andre_silva
NXP Employee
NXP Employee

Hi Sheldon,

for the 2D API I only found the one attached, it will be available on the next gpu sdk release. Hope it helps you.

regards,

Andre

0 件の賞賛
返信
3,734件の閲覧回数
sheldonrucker
Contributor III

Thank you Andre!  I'm sure this will help.

Sheldon

0 件の賞賛
返信
3,734件の閲覧回数
andre_silva
NXP Employee
NXP Employee

no problem, good luck =)

0 件の賞賛
返信
3,734件の閲覧回数
andre_silva
NXP Employee
NXP Employee

I´m going to look for it and let you know

0 件の賞賛
返信