linux 2.6.31 kernel patch for Micron NAND MT29F1G08ABAFA(M78a)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

linux 2.6.31 kernel patch for Micron NAND MT29F1G08ABAFA(M78a)

ソリューションへジャンプ
1,812件の閲覧回数
rudrar
Contributor I

We are using IMX25. And linux version 2.6.31. We are migrating the NAND from  Micron MT29F1G08ABADA to MT29F1G08ABAFA. The new NAND is not supported in 2.6.31 version. I need a patch that allows support of new NAND. How can I go ahead in this?

Do I need to do changes in bootloader also for this?

0 件の賞賛
返信
1 解決策
1,694件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

2.6.31 kernel is no longer supported. You can try the latest mainline kernel (4.16) on i.MX25 instead.

Regards,

Fabio Estevam

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,695件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

2.6.31 kernel is no longer supported. You can try the latest mainline kernel (4.16) on i.MX25 instead.

Regards,

Fabio Estevam

0 件の賞賛
返信