linux 2.6.31 kernel patch for Micron NAND MT29F1G08ABAFA(M78a)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

linux 2.6.31 kernel patch for Micron NAND MT29F1G08ABAFA(M78a)

Jump to solution
1,805 Views
rudrar
Contributor I

We are using IMX25. And linux version 2.6.31. We are migrating the NAND from  Micron MT29F1G08ABADA to MT29F1G08ABAFA. The new NAND is not supported in 2.6.31 version. I need a patch that allows support of new NAND. How can I go ahead in this?

Do I need to do changes in bootloader also for this?

0 Kudos
Reply
1 Solution
1,687 Views
fabio_estevam
NXP Employee
NXP Employee

2.6.31 kernel is no longer supported. You can try the latest mainline kernel (4.16) on i.MX25 instead.

Regards,

Fabio Estevam

View solution in original post

0 Kudos
Reply
1 Reply
1,688 Views
fabio_estevam
NXP Employee
NXP Employee

2.6.31 kernel is no longer supported. You can try the latest mainline kernel (4.16) on i.MX25 instead.

Regards,

Fabio Estevam

0 Kudos
Reply