linux 2.6.31 kernel patch for Micron NAND MT29F1G08ABAFA(M78a)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

linux 2.6.31 kernel patch for Micron NAND MT29F1G08ABAFA(M78a)

跳至解决方案
1,835 次查看
rudrar
Contributor I

We are using IMX25. And linux version 2.6.31. We are migrating the NAND from  Micron MT29F1G08ABADA to MT29F1G08ABAFA. The new NAND is not supported in 2.6.31 version. I need a patch that allows support of new NAND. How can I go ahead in this?

Do I need to do changes in bootloader also for this?

0 项奖励
回复
1 解答
1,717 次查看
fabio_estevam
NXP Employee
NXP Employee

2.6.31 kernel is no longer supported. You can try the latest mainline kernel (4.16) on i.MX25 instead.

Regards,

Fabio Estevam

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,718 次查看
fabio_estevam
NXP Employee
NXP Employee

2.6.31 kernel is no longer supported. You can try the latest mainline kernel (4.16) on i.MX25 instead.

Regards,

Fabio Estevam

0 项奖励
回复