imx8qxp chromium-ozone-wayland build fail

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8qxp chromium-ozone-wayland build fail

4,229件の閲覧回数
darsh_dev
Contributor V

Hi 

I am try to build chromium-ozone-wayland in 5.4.47 zeus release for imx8qxp by adding CORE_IMAGE_EXTRA_INSTALL += "chromium-ozone-wayland" in local.conf file.

it fails to compile gn-native package.

../../../tools/gn/src/base/logging.h:14:10: fatal error: 'string_view' file not found

Summary: 1 task failed:
/home/imx8/NXP/L5_4_47/sources/meta-browser/recipes-browser/chromium/gn-native_83.0.4103.116.bb:do_compile

Please find attached the fail log.

Please help what going wrong. how can resolve the above issue?

Regards,

Arjun

0 件の賞賛
返信
4 返答(返信)

4,215件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,

  Refer to the link to solve the problem, please!

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Adding-Chromium-to-L5-4-24-2-1-0-I-MX8MQ...

 

Have a nice day!

B.R,

weidong

0 件の賞賛
返信

4,201件の閲覧回数
darsh_dev
Contributor V

Hi @weidong_sun ,

No luck by adding mesa in chromium-ozone-wayland_%.bbappend.

still, gn-native do_compile fail.

../../../tools/gn/src/base/logging.h:14:10: fatal error: 'string_view' file not found

Summary: 1 task failed:
/home/imx8/NXP/L5_4_47/sources/meta-browser/recipes-browser/chromium/gn-native_83.0.4103.116.bb:do_compile

Note: we are working on the imx-5.4.47-2.2.0 Zeus release.

Regards,

Arjun

0 件の賞賛
返信

3,753件の閲覧回数
Larry69
Contributor I

when I try to run ./out/Debug/chrome --no-sandbox, I get errors.

0 件の賞賛
返信

3,788件の閲覧回数
jran
Contributor II

Hello @darsh_dev , did you ever manage to solve this?

I'm facing the same issue when trying to build Chromium.

0 件の賞賛
返信