imx8mnevk modify uboot to flash image over ethernet

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx8mnevk modify uboot to flash image over ethernet

1,091件の閲覧回数
cschmidt
Contributor I

I am developing an image with yocto and the imx8mnevk board. It is realy exhausting to:

1. turn the board off

2. modifying the dips switch

3. turn on

4. flash

5. turn off

6. modifying the dips switch

7. turn on

Is there a more practical way? I my point of view i already flashed the bootloader uboot and uboot should be capable of flashing just a new firmware. I search for a solution to modify uboot to load an image via network but didn't find anything.

any ideas?

0 件の賞賛
返信
1 返信

1,051件の閲覧回数
Yuri
NXP Employee
NXP Employee

cschmidt@kt-elektronik.de 

Hello,

  Customers can use NFS - by default, in U-boot configuration, rootfs is mounted on NFS.

Also, U-boot supports TFTP. Consult with NXP Linux BSP documentation (i.MX Linux User's

Guide).

Regards,

Yuri.

0 件の賞賛
返信