imx8mnevk modify uboot to flash image over ethernet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8mnevk modify uboot to flash image over ethernet

1,009 次查看
cschmidt
Contributor I

I am developing an image with yocto and the imx8mnevk board. It is realy exhausting to:

1. turn the board off

2. modifying the dips switch

3. turn on

4. flash

5. turn off

6. modifying the dips switch

7. turn on

Is there a more practical way? I my point of view i already flashed the bootloader uboot and uboot should be capable of flashing just a new firmware. I search for a solution to modify uboot to load an image via network but didn't find anything.

any ideas?

0 项奖励
回复
1 回复

969 次查看
Yuri
NXP Employee
NXP Employee

cschmidt@kt-elektronik.de 

Hello,

  Customers can use NFS - by default, in U-boot configuration, rootfs is mounted on NFS.

Also, U-boot supports TFTP. Consult with NXP Linux BSP documentation (i.MX Linux User's

Guide).

Regards,

Yuri.

0 项奖励
回复