1、can this fsl-image-qt5-validation-imx-imx8mqevk.sdcard be burnt in SDcard?
2、SDcard file system is exFAT?
3、how to make a boot SDcard? I followed the user manual but failed
已解决! 转到解答。
Hello,
1.- Yes, it is an image ready to be flashed on your SD/MMC.
2.- The image layout is as following:
3.- You'll need to follow the i.MX_Linux_User's_Guide.pdf be it using UUU, section 4.2 Universal update utility, or by using a PC with Linux OS, section 4.3.2 Copying the full SD card image.
Hope this helps
Regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello,
1.- Yes, it is an image ready to be flashed on your SD/MMC.
2.- The image layout is as following:
3.- You'll need to follow the i.MX_Linux_User's_Guide.pdf be it using UUU, section 4.2 Universal update utility, or by using a PC with Linux OS, section 4.3.2 Copying the full SD card image.
Hope this helps
Regards,
Aldo.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------