imx8:questions about how to make a boot SDcard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx8:questions about how to make a boot SDcard

Jump to solution
2,805 Views
1304662033
Contributor II

1、can this fsl-image-qt5-validation-imx-imx8mqevk.sdcard  be burnt in SDcard?

2、SDcard file system is exFAT?

3、how to make a boot SDcard? I followed the user manual but failed

0 Kudos
Reply
1 Solution
2,567 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,


1.- Yes, it is an image ready to be flashed on your SD/MMC.

2.- The image layout is as following:

 pastedImage_1.png

3.- You'll need to follow the i.MX_Linux_User's_Guide.pdf be it using UUU, section 4.2 Universal update utility, or by using a  PC with Linux OS, section 4.3.2 Copying the full SD card image.

 

Hope this helps

Regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,568 Views
AldoG
NXP TechSupport
NXP TechSupport

Hello,


1.- Yes, it is an image ready to be flashed on your SD/MMC.

2.- The image layout is as following:

 pastedImage_1.png

3.- You'll need to follow the i.MX_Linux_User's_Guide.pdf be it using UUU, section 4.2 Universal update utility, or by using a  PC with Linux OS, section 4.3.2 Copying the full SD card image.

 

Hope this helps

Regards,

Aldo.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply