imx8 mini MIPI video 1Gbps clock setting question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx8 mini MIPI video 1Gbps clock setting question

390 次查看
sutton_kim
Contributor II

I'm trying to change the D-Phy setting on my imx8 mini from 1.5G bps to 1Gbps D-PHY. 
However, CLKCTRL_DPHY_SEL_1G and CLKCTRL_PLLBYPASS are set to the same 29 bits. In the reference manual, CLKCTRL_PLLBYPASS is set to 27 bits. However, when I change CLKCTRL_PLLBYPASS to 27 bits, I get kernel panic and imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi errors. Can you tell me the cause?

below is in sec-dsim.c define part. 

#define CLKCTRL_TXREQUESTHSCLK BIT(31)
#define CLKCTRL_DPHY_SEL_1G BIT(29)
#define CLKCTRL_DPHY_SEL_1P5G (0x0 << 29)
#define CLKCTRL_ESCCLKEN BIT(28)
#define CLKCTRL_PLLBYPASS BIT(29)
#define CLKCTRL_BYTECLKSRC_DPHY_PLL REG_PUT(0, 26, 25)
#define CLKCTRL_BYTECLKEN BIT(24)
#define CLKCTRL_SET_LANEESCCLKEN(x) REG_PUT(x, 23, 19)
#define CLKCTRL_SET_ESCPRESCALER(x) REG_PUT(x, 15, 0)

sec-dsim.c sec_mipi_dsim_config_clkctrl()
static void sec_mipi_dsim_config_clkctrl(struct sec_mipi_dsim *dsim)
{
uint32_t clkctrl = 0, data_lanes_en;
uint32_t byte_clk, esc_prescaler;
 
clkctrl |= CLKCTRL_TXREQUESTHSCLK;
 
/* using 1.5Gbps PHY */
clkctrl |= CLKCTRL_DPHY_SEL_1P5G;
 
clkctrl |= CLKCTRL_ESCCLKEN;
 
clkctrl &= ~CLKCTRL_PLLBYPASS;
 
clkctrl |= CLKCTRL_BYTECLKSRC_DPHY_PLL;
 
clkctrl |= CLKCTRL_BYTECLKEN;
 
data_lanes_en = (0x1 << dsim->lanes) - 1;
clkctrl |= CLKCTRL_SET_LANEESCCLKEN(0x1 | data_lanes_en << 1);
 
/* calculate esc prescaler from byte clock:
* EscClk = ByteClk / EscPrescaler;
*/
byte_clk = dsim->bit_clk >> 3;
esc_prescaler = DIV_ROUND_UP(byte_clk, MAX_ESC_CLK_FREQ);
clkctrl |= CLKCTRL_SET_ESCPRESCALER(esc_prescaler);
 
dsim_write(dsim, clkctrl, DSIM_CLKCTRL);
}
 
 
Starting kernel ...
 
[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 5.4.210 (oe-user@oe-host) (gcc version 9.3.0 (GCC)) #1 SMP PREEMPT Tue Sep 20 15:11:49 UTC 2022
[    0.000000] Machine model: FSL i.MX8MM LPDDR4 Titan board
[    0.000000] earlycon: ec_imx6q0 at MMIO 0x0000000030890000 (options '115200')
[    0.000000] printk: bootconsole [ec_imx6q0] enabled
[    0.072576] No BMan portals available!
[    0.073876] No QMan portals available!
[    0.217625] imx_sec_dsim_drv 32e10000.mipi_dsi: Failed to attach bridge: 32e10000.mipi_dsi
[    0.225963] imx_sec_dsim_drv 32e10000.mipi_dsi: failed to bind sec dsim bridge: -517
[    0.364200] *!*!*!*!* Reseting Panel
[    0.397697] *!*!*!*!* Version 3.0 tianma_panel_enable
[    0.571499] imx6q-pcie 33800000.pcie: host bridge /soc@0/pcie@33800000 ranges:
[    0.571525] imx6q-pcie 33800000.pcie:    IO 0x1ff80000..0x1ff8ffff -> 0x00000000
[    0.571539] imx6q-pcie 33800000.pcie:   MEM 0x18000000..0x1fefffff -> 0x18000000
[    0.671435] imx_sec_dsim_drv 32e10000.mipi_dsi: wait payload tx done time out
[    0.671451] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI ff
[    0.673521] imx6q-pcie 33800000.pcie: Link up
[    0.771439] imx6q-pcie 33800000.pcie: Link up
[    0.771444] imx6q-pcie 33800000.pcie: Link up, Gen2
[    0.771566] imx6q-pcie 33800000.pcie: PCI host bridge to bus 0000:00
[    0.771573] pci_bus 0000:00: root bus resource [bus 00-ff]
[    0.771578] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
[    0.771582] pci_bus 0000:00: root bus resource [mem 0x18000000-0x1fefffff]
[    0.771605] pci 0000:00:00.0: [16c3:abcd] type 01 class 0x060400
[    0.771625] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x000fffff]
[    0.771636] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x0000ffff pref]
[    0.771678] pci 0000:00:00.0: supports D1
[    0.771683] pci 0000:00:00.0: PME# supported from D0 D1 D3hot D3cold
[    0.773472] pci 0000:01:00.0: [1172:0000] type 00 class 0xff0000
[    0.773570] pci 0000:01:00.0: reg 0x10: [mem 0x00000000-0x00007fff 64bit pref]
[    0.773612] pci 0000:01:00.0: reg 0x18: [mem 0x00000000-0x00007fff 64bit pref]
[    0.773654] pci 0000:01:00.0: reg 0x20: [mem 0x00000000-0x000fffff 64bit pref]
[    0.775539] pci 0000:00:00.0: BAR 0: assigned [mem 0x18000000-0x180fffff]
[    0.775548] pci 0000:00:00.0: BAR 15: assigned [mem 0x18100000-0x182fffff pref]
[    0.775554] pci 0000:00:00.0: BAR 6: assigned [mem 0x18300000-0x1830ffff pref]
[    0.775563] pci 0000:01:00.0: BAR 4: assigned [mem 0x18100000-0x181fffff 64bit pref]
[    0.775599] pci 0000:01:00.0: BAR 0: assigned [mem 0x18200000-0x18207fff 64bit pref]
[    0.775634] pci 0000:01:00.0: BAR 2: assigned [mem 0x18208000-0x1820ffff 64bit pref]
[    0.775668] pci 0000:00:00.0: PCI bridge to [bus 01-ff]
[    0.775675] pci 0000:00:00.0:   bridge window [mem 0x18100000-0x182fffff pref]
[    0.927444] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    0.927459] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 0
[    1.183439] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    1.183448] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 1
[    1.439435] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    1.439444] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 2
[    1.695445] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    1.695453] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 3
[    1.951433] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    1.951441] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 4
[    2.207433] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    2.207441] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 5
[    2.463443] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    2.463451] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 6
[    2.719441] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    2.719449] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 7
[    2.975451] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    2.975459] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 8
[    3.231430] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    3.231438] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI 9
[    3.487458] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    3.487466] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI a
[    3.743437] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    3.743445] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI b
[    3.999435] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    3.999443] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI c
[    4.255436] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    4.255444] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI d
[    4.511455] imx_sec_dsim_drv 32e10000.mipi_dsi: wait pkthdr tx done time out
[    4.511464] panel-tianma-tm043yvgp44 32e10000.mipi_dsi.0: [drm:tianma_panel_enable] *ERROR* Tianma Panel Error Writing DSI e
[    4.511732] SError Interrupt on CPU2, code 0xbf000002 -- SError
[    4.511735] CPU: 2 PID: 51 Comm: kworker/2:1 Not tainted 5.4.210 #1
[    4.511736] Hardware name: FSL i.MX8MM LPDDR4 Titan board (DT)
[    4.511738] Workqueue: events deferred_probe_work_func
[    4.511741] pstate: 60000005 (nZCv daif -PAN -UAO)
[    4.511742] pc : _raw_spin_unlock_irq+0x1c/0x48
[    4.511744] lr : wait_for_completion_timeout+0x8c/0x110
[    4.511745] sp : ffff800012f1b2d0
[    4.511746] x29: ffff800012f1b2d0 x28: ffff800010fe8098
[    4.511749] x27: ffff0000ff7fcee8 x26: ffff800011305910
[    4.511752] x25: ffff800011294638 x24: ffff0000f8425580
[    4.511755] x23: 0000000000000002 x22: ffff0000f8425580
[    4.511759] x21: ffff0000f45d9df8 x20: ffff0000f45d9df0
[    4.511762] x19: 000000000000003f x18: 0000000000000020
[    4.511765] x17: 0000000000000000 x16: 0000000000000000
[    4.511768] x15: ffff800012a43000 x14: 205d656c62616e65
[    4.511771] x13: 5f6c656e61705f61 x12: 6d6e6169743a6d72
[    4.511774] x11: 645b203a302e6973 x10: 645f6970696d2e30
[    4.511777] x9 : 3030303165323320 x8 : 0000000000000000
[    4.511780] x7 : 0000000000000000 x6 : 0000000003e1c9c4
[    4.511783] x5 : 0000000000000001 x4 : ffff0000f45d9e00
[    4.511786] x3 : ffff0000f8425580 x2 : ffff800012f1b328
[    4.511789] x1 : ffff0000f8425580 x0 : 0000000100000001
[    4.511793] Kernel panic - not syncing: Asynchronous SError Interrupt
[    4.511795] CPU: 2 PID: 51 Comm: kworker/2:1 Not tainted 5.4.210 #1
[    4.511797] Hardware name: FSL i.MX8MM LPDDR4 Titan board (DT)
[    4.511798] Workqueue: events deferred_probe_work_func
[    4.511800] Call trace:
[    4.511801]  dump_backtrace+0x0/0x188
[    4.511803]  show_stack+0x14/0x20
[    4.511804]  dump_stack+0xb4/0x110
[    4.511805]  panic+0x15c/0x328
[    4.511806]  nmi_panic+0x84/0x88
[    4.511807]  arm64_serror_panic+0x74/0x80
[    4.511809]  do_serror+0x80/0x138
[    4.511810]  el1_error+0x84/0xf8
[    4.511811]  _raw_spin_unlock_irq+0x1c/0x48
[    4.511813]  sec_mipi_dsim_host_transfer+0x1a4/0x428
[    4.511814]  mipi_dsi_device_transfer.isra.0+0x48/0x58
[    4.511816]  mipi_dsi_generic_write+0x68/0xa0
[    4.511817]  tianma_panel_enable+0x114/0x320
[    4.511818]  drm_panel_enable+0x24/0x38
[    4.511820]  sec_mipi_dsim_bridge_enable+0x328/0x470
[    4.511821]  drm_atomic_bridge_enable+0x4c/0x68
[    4.511823]  drm_atomic_helper_commit_modeset_enables+0x11c/0x230
[    4.511825]  lcdif_drm_atomic_commit_tail+0x2c/0x68
[    4.511826]  commit_tail+0x9c/0x188
[    4.511827]  drm_atomic_helper_commit+0x154/0x168
[    4.511829]  drm_atomic_commit+0x48/0x58
[    4.511830]  drm_client_modeset_commit_atomic.isra.0+0x174/0x230
[    4.511832]  drm_client_modeset_commit_force+0x58/0x190
[    4.511833]  drm_fb_helper_restore_fbdev_mode_unlocked+0x70/0xd0
[    4.511835]  drm_fb_helper_set_par+0x2c/0x58
[    4.511836]  fbcon_init+0x244/0x4c8
[    4.511837]  visual_init+0xac/0x100
[    4.511839]  do_bind_con_driver+0x1cc/0x3a0
[    4.511840]  do_take_over_console+0x13c/0x1f8
[    4.511841]  do_fbcon_takeover+0x6c/0xe0
[    4.511843]  fbcon_fb_registered+0xfc/0x110
[    4.511844]  register_framebuffer+0x1e8/0x330
[    4.511846]  __drm_fb_helper_initial_config_and_unlock+0x2d0/0x470
[    4.511847]  drm_fbdev_client_hotplug+0xd4/0x188
[    4.511849]  drm_fbdev_generic_setup+0x98/0x140
[    4.511850]  imx_drm_bind+0x100/0x150
[    4.511852]  try_to_bring_up_master+0x164/0x1c8
[    4.511853]  __component_add+0xa0/0x168
[    4.511854]  component_add+0x10/0x18
[    4.511855]  imx_sec_dsim_probe+0x4c/0x70
[    4.511857]  platform_drv_probe+0x50/0xa0
[    4.511858]  really_probe+0xd4/0x318
[    4.511859]  driver_probe_device+0x54/0xe8
[    4.511861]  __device_attach_driver+0x80/0xb8
[    4.511862]  bus_for_each_drv+0x74/0xc0
[    4.511863]  __device_attach+0xf0/0x180
[    4.511865]  device_initial_probe+0x10/0x18
[    4.511866]  bus_probe_device+0x90/0x98
[    4.511867]  deferred_probe_work_func+0x64/0x98
[    4.511869]  process_one_work+0x1b4/0x328
[    4.511870]  worker_thread+0x1f0/0x420
[    4.511871]  kthread+0x138/0x158
[    4.511873]  ret_from_fork+0x10/0x1c
[    4.511990] SMP: stopping secondary CPUs
[    4.511991] Kernel Offset: disabled
[    4.511993] CPU features: 0x00002,2000200c
[    4.511994] Memory Limit: none
 
 

 

0 项奖励
回复
1 回复

295 次查看
lydia_ziegler
NXP Employee
NXP Employee

Hi @sutton_kim 

I found an article that may help you.  Can you take a look at this:

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Setting-i-MX8M-Mini-and-Nano-MIPI-DPHY-C...

 

Thanks,

Lydia

0 项奖励
回复