imx6ull secure-boot enabling

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ull secure-boot enabling

2,421 次查看
jay_kaneria
Contributor I

Hi, 

I have enabled secure-boot option in defconfig of u-boot, signed image with appropriate certificates. Now, i am trying to flash the image on board using mfgtool. After flashing the image, when i check the hab_status, i am getting hab events.

Now when i flash the same signed image using "imx_usb_loader" like mentioned here "https://community.nxp.com/docs/DOC-94117 ", i am not getting any hab events in  'Serial Download Mode'. My signed u-boot image works properly in 'Serial Download Mode' but agains gives hab events when i switch the mode.

I am suspecting problem with my "ucl.xml" file in mfgtool. I am attaching the "ucl.xml" file here.

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

2,322 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jay

one can refer to

Secure Boot and HAB document for i.MX6ULL 

also additional document was sent via mail.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复