imx6ull error about burning by using mfgtool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ull error about burning by using mfgtool

3,756 Views
ida_jiang
Contributor III

Hello,

      I'm using imx6ull board and have built a yocto project by setting bitbake fsl-image-machine-test. And I want to use mfgtool to burn files to imx6ull's nand. The cfg.ini is as follows:

       [profiles]
       chip = Linux
       [platform]
       board = SabreSD
       [LIST]
       name = NAND Flash

     

       And the file's location has no problem. As for the mfgtool.vbs, I also had changed:

Set wshShell = CreateObject("WScript.shell")
wshShell.run "mfgtool2.exe -c ""linux"" -l ""NAND Flash"" -s ""sxuboot=sabreauto""  -s ""sxdtb=sabreauto"" -s ""6ulluboot=14x14evk"" -s ""6ulldtb=14x14-evk"" -s ""board=sabreauto"" -s ""nand=nand"" -s ""nanddtb=gpmi-weim"" -s ""part_uboot=0"" -s ""part_kernel=1"" -s ""part_dtb=2"" -s ""part_rootfs=3""   "
Set wshShell = Nothing

      When I clicked the program's start, it showed:

mfgtool_error.png

      How can I deal with it? Hope your help!

Tags (3)
0 Kudos
Reply
14 Replies

3,529 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ida,

The Demo images you need as following:

L4.1.15_2.0.0_iMX6ULL Demo

https://www.nxp.com/webapp/sps/download/preDownload.jsp 

i.MX 6UltraLite Linux Binary Demo Files and Linux BSP Documentation

L3.14.38_iMX6UL 

Have a nice day

Rita

0 Kudos
Reply

3,529 Views
ida_jiang
Contributor III

Hi Rita ,

     I used the L4.1.14_2.0.0_ga's demo for imx6ull and burned the image to nand by uuu & mfgtool. Both of them can't burn successfully. And the log was as follows:

3.png

    As for mfgtool, it would get stuck at "jump OS linux".

    Have you made any progress?

Best Regards !

Ida

0 Kudos
Reply

3,529 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

which version of mfgtool are you using?

0 Kudos
Reply

3,529 Views
ida_jiang
Contributor III

 Hi Rita,

      Thank you for your reply.

      ① I'm using the mfgtool for L4.1.15_2.0.0_ga_imx6ul and using the mfgtool-yocto-mx-evk-nand.vbs to burn the image. The files I used are from this demo.

      ② As for the uuu(1.2.89) , the files are also from the demo. And I did "$ sudo ./uuu example_kernel_nand.uuu". The file "example_kernel_nand.uuu" is from L4.14.98_ga's demo. I got these demo from the official website.

      ③ It seems that the latest release (1.3.89) of uuu can support the nand with nandbcb command. But at present , the uboot can not support this new command. There will be some change about uboot  for this situation?

Best Regards!

Ida

0 Kudos
Reply

3,529 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ida,

The NAND rework need to remove the QSPI(U303), C318, R324, and SHORT the R324.

For the L4.1.15_2.0.0_ga_imx6ul you can use the mfgtool-yocto-mx-evk-nand.vbs to burn the image.

For the L4.14.98_ga there are mfgtool and uuu for you to use. Manufacturing Toolkit for Linux L4.9.88_2.0.0 i.MX6,7 BSP. uuu you can use the 1.2.35.

Have a nice day

Rita

0 Kudos
Reply

3,529 Views
ida_jiang
Contributor III

Hi Rita,

     Thank you for your reply. 

     Actually I have try the  mfgtool that you said to burn. But I can't do it successfully. Can you help me check my operation steps?

(1) L4.1.15_2.0.0_ga

① Download the L4.1.15_2.0.0_ga_imx6ul from official website and change nothing.

② Open the mfgtool-yocto-mx-evk-nand.vbs and use it directly.

(2) L4.9.88_2.0.0_ga

① Download from official website. Delete the zImage & imx6ullevk-gpmi-weim.dtb & u-boot-imx6ullevk_nand.imx and use my files which have changed to the name of the deleted files.

② Open the mfgtool-yocto-mx-evk-nand.vbs and use it to burn image.

      And what is your test hardware environment? 

      And where can I get the 1.2.35 uuu?

Best Regards!

Ida

0 Kudos
Reply

3,529 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

I am using the i.MX6ULL EVK board without the nand on board. Could you send your error messages to us?

0 Kudos
Reply

3,529 Views
ida_jiang
Contributor III

The logs using two mfgtools are here.

0 Kudos
Reply

3,529 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ida,

You can contact with Kane I see he give you reply in another thread.

Have a nice day

Rita

0 Kudos
Reply

3,529 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ida,

I will do test late, and will give you reply next Monday.

Have a nice weekend

Best Regards

Rita

0 Kudos
Reply

3,529 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Ida,

Could you send me your steps? I am do our new BSP test these days, so I will work for you late today. Sorry about the late reply.

Have a nice day

Rita

0 Kudos
Reply

3,529 Views
ida_jiang
Contributor III

Hi Rita,

     Thanks for you reply. And I also want to know that weather after L4.9.123, MFGtool cannot be used ?

0 Kudos
Reply

3,529 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Now the newer BSP version, use the UUU tool, I will try it, and will tell you details

0 Kudos
Reply

3,529 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which version of BSP are you using?

0 Kudos
Reply