imx6ul evk version B & C

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ul evk version B & C

2,762 次查看
healy
NXP Employee
NXP Employee

I have 6UL EVK version B, but I see the AN5229, in the AN, user case for kernel debug is with version C,

May I know the difference? can I use the versionB EVK to debug linux knernel source code with Dstream in DS-5?

thanks  a  lot! 

6 回复数

2,623 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Healy

differencies between B and C are described on p.1 schematic

Table"Revision History"

Schematics (1)
MCIMX6UL-EVK_DESIGNFILES

i.MX6UltraLite Evaluation Kit|NXP 

>can I use the versionB EVK to debug linux knernel source code with Dstream in DS-5?

yes, differencies between B and C are changing some resistors and adding components for

passing fcc tests and not affect jtag debug operations.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,623 次查看
healy
NXP Employee
NXP Employee

Hi Igorpadykov

thank you for your support!

Now I can connect to 6ULEVK  and run kernel code at DS-5 with DStream

but I found that after connect to 6ULEVK, I can't input any command at termial, had you encoutnered the issue?

thanks a lot!

0 项奖励
回复

2,623 次查看
igorpadykov
NXP Employee
NXP Employee

please check AN5229 ARM DS-5 Development Studio Debug i.MX6UL-EVK

https://www.nxp.com/docs/en/application-note/AN5229.pdf 


Best regards
igor

2,623 次查看
healy
NXP Employee
NXP Employee

Hi Igorpadykov

I had followed the AN and now I can debug kernel( can run/stop & step/step into, view variable successfully) in DS-5,

issue I encountered is  - I can't input any command in terminal after perform debug running command!

I plan to use "insmod" command to invoke my device dirver & debug it. but I found I can't input any command in terminal after "connect the EVK & debug run"

had you any idea about that?

Thanks you so much!

0 项奖励
回复

2,623 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Healy

suggest to create new threads for new questions.

Best regards
igor

0 项奖励
回复

2,623 次查看
healy
NXP Employee
NXP Employee

Hi Igorpadykov

I hand modify the patch code mensioned at AN5299 to linux kernel version 4.1.15

now the problem be fixed.

thank you so much!

0 项奖励
回复