How to rebuild kernel Source in imx6ulevk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to rebuild kernel Source in imx6ulevk

1,693 Views
nagaprasadvasam
Contributor III

Hi,

   i have downloaded freescale BSP for imx6ulevk.booted kernel using yocto build using bitbake command.i need to edit driver in source code and re-compile it how can i re-build kernel source can any one help me.

Thanks & Regards,

Prasad.

Labels (3)
0 Kudos
Reply
2 Replies

1,542 Views
nagaprasadvasam
Contributor III

Hi  igor,

         I need to communicate 4g module with imx6ulevk board, but when i am connecting through it ,it was not detecting any node in /dev ,

         when i am connecting it is showing as follows,

         usb 1-1: new high-speed USB device number 4 using ci_hdrc

         But i need to communicate module  with board can u please help me how to detect node in /dev folder

Thanks & Regards,

Prasad.

0 Kudos
Reply

1,542 Views
igorpadykov
NXP Employee
NXP Employee

Hi Prasad

may be helpful to look on

i.MX Yocto Project: How can I (quickly) modify the kernel and test it? 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply