imx6ul Dual ethernet connector question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6ul Dual ethernet connector question

1,187 Views
zhangbin_eos
Contributor III

hi

board is imx6ul-14x14-evk.

Does the board's dual ethernet support independent work?
Is it possible to choose one of the ethernets to work independently, or two ethernets to work at the same time?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,046 Views
rakesh_patel
Senior Contributor I

Hi zhangbin.eos@foxmail.com,

Yes, it is possible to use the dual ethernet port independently as well as both the ethernets at the same time.

To use only a single Ethernet, we can change the device tree node and disable the ethernet which you don't want to use.

Regards,

Rakesh

0 Kudos
Reply

1,046 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

Which BSP is running on your board?

0 Kudos
Reply