Eyption rfs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Eyption rfs

2,079 次查看
PramodKumar
Contributor IV

Hii Team,

I need to encrypt the imx6ul root file system i studied about this from the below reference but it is not makes me understandable can anybody provide me clear document to work on it from scratch on-wards .

Ref :- Encrypt Your Root Filesystem | Linux Journal 

Regards ,

Pramod

标签 (3)
0 项奖励
回复
3 回复数

1,998 次查看
Yuri
NXP Employee
NXP Employee

Hello.

  I've sent You some information directly. Hope it helps.


Have a great day,
Yuri.

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,998 次查看
PramodKumar
Contributor IV

Hii yuri ,

Where you have sent me the docs for the same ?

Thanks ,

Pramod

0 项奖励
回复

1,998 次查看
Yuri
NXP Employee
NXP Employee

[email protected]  - this e-mail was used to send the files.

~Yuri.

0 项奖励
回复