imx6ul Dual ethernet connector question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6ul Dual ethernet connector question

1,180 次查看
zhangbin_eos
Contributor III

hi

board is imx6ul-14x14-evk.

Does the board's dual ethernet support independent work?
Is it possible to choose one of the ethernets to work independently, or two ethernets to work at the same time?

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,039 次查看
rakesh_patel
Senior Contributor I

Hi zhangbin.eos@foxmail.com,

Yes, it is possible to use the dual ethernet port independently as well as both the ethernets at the same time.

To use only a single Ethernet, we can change the device tree node and disable the ethernet which you don't want to use.

Regards,

Rakesh

0 项奖励
回复

1,039 次查看
Rita_Wang
NXP TechSupport
NXP TechSupport

Which BSP is running on your board?

0 项奖励
回复