imx6sl ddr3 failed(yocto)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6sl ddr3 failed(yocto)

1,254件の閲覧回数
indukkim
Contributor I

Hi All,

We got a board with DDR3, we used the spreadsheet for

i.MX6 sololite for generating a DCD table. (imximage.cfg)

Pass the DDR Stress test.
But download failed with the mfgtools. (stop the "Jumping to OS image.)


Detail Info

DDR3 : Samsung KB1G1646G-BCK0

spreadsheet : MX6SL_MMDC_DDR3_register_programming_aid_v0[1].4.xlsx

Build uboot: yocto (u-boot-imx 2013.04-r0)


Please help us.

ラベル(2)
0 件の賞賛
返信
1 返信

961件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Induk

for new board I would suggest to use more mature

and well documented product ltib/mfg tool on link below

IMX_6SL_MFG_TOOL

L3.0.35_4.1.0_ER_SOURCE_BSP :

When board will boot OK with these packages I would recommend

go to yocto.

For new board you should rebuid MFG Tool firmware

(initramfs.cpio.gz.uboot) with new DDR settings.

Check sect.3.8 Building Manufacturing Firmware

i.MX_6SoloLite_EVK_Linux_User's_Guide.pdf

These documents you can find in Doc Bundle below

L3.0.35_4.1.0_LINUX_DOCS

Good starting point would be test board with SDK,

booting with small test inages

i.MX 6Series Platform SDK

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信