imx6q starting kernel hangs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q starting kernel hangs

6,711 次查看
taowang1
Contributor I

Hi,all:

I encounter one problem recently.After power on, after uboot finishes, the kernel hangs..

I also try the method(chapter 1.1 and 1.2 ) by:  Common Problems - Linux kernel doesnt boot - RidgeRun Developer Connection

but problem still exists.

Because the uboot is supplied by the third parner ,I don't know  why the buled words occurs.

The platform information is as follows:

cpu: imx6q

board: customized board based on sabreAuto

os: android kk4.4.2_1.0.0,kernel:Linux 3.0.35

The following is the log(board is marked manualy on purpose ):

U-Boot 2014.04-00024-g5895096 (Apr 27 2016 - 23:57:08)

CPU:   Freescale i.MX6Q rev1.5 at 792 MHz

CPU:   Temperature 16 C, calibration data: 0x5744d47d

Reset cause: POR

Board: XXXXXXXX Board ==>(note:XXXX is marked manually on purpose)

I2C:   ready

DRAM:  2 GiB

MMC:   FSL_SDHC: 0, FSL_SDHC: 1

SF: Detected S25FL164A with page size 256 Bytes, erase size 64 KiB, total 8 MiB

*** Warning - bad CRC, using default environment

No panel detected: default to Hannstar-XGA

Display: Hannstar-XGA (1024x768)

In:    serial

Out:   serial

Err:   serial

unsupported boot devices

check_and_clean: reg 0, flag_set 0

Recovery key pressed

Fastboot: Recovery command file founded!

Unsupported bootup device for recovery: dev: 5

flash target is MMC:1

Net:   Board Net Initialization Failed

No ethernet found.

Normal Boot

Hit '>' key to stop autoboot:  0

mmc1(part 0) is current device

MMC read: dev # 1, block # 2048, count 14336 ... 14336 blocks read: OK

booti 0x12000000

kernel   @ 10808000 (4753788)

ramdisk  @ 11800000 (499839)

kernel cmdline:

        use boot.img command line:

        console=ttymxc0,115200 androidboot.console=ttymxc0 vmalloc=400M init=/init video=mxcfb0:dev=lc      d,AT070-WVGA,if=RGB24,bpp=32 video=mxcfb1:dev=hdmi,1920x1080M@60,if=RGB24,bpp=32 video=mxcfb2:off fbme      m=10M,28M  fec_mac=1E:ED:19:27:1A:B3 androidboot.hardware=freescale androidboot.serialno=202091d4e3174      a01

No gpc device node -9, force to ldo-enable.

Starting kernel ...

waiting for your reply,Thanks!

0 项奖励
回复
9 回复数

4,772 次查看
taowang1
Contributor I

Hi,all,

     I knew the problem resides in the gpc,If I delete the gpc node in device tree for the image of the third partner

The same phenomenon occurs。The gpc node is defined as follows:

gpc@020dc000 {
compatible = "fsl,imx6q-gpc";
reg = <0x20dc000 0x4000>;
interrupts = <0x0 0x59 0x4 0x0 0x5a 0x4>;
clocks = <0x2 0x7a 0x2 0x4a 0x2 0x79 0x2 0x1a 0x2 0x8f 0x2 0xa8 0x2 0x3e>;
clock-names = "gpu3d_core", "gpu3d_shader", "gpu2d_core", "gpu2d_axi", "openvg_axi", "vpu_axi", "ipg";
pu-supply = <0x12>;
fsl,cpu_pupscr_sw2iso = <0xf>;
fsl,cpu_pupscr_sw = <0xf>;
fsl,cpu_pdnscr_iso2sw = <0x1>;
fsl,cpu_pdnscr_iso = <0x1>;
};

If I delete the "pu-supply = <0x12>",the kernel can walk to "atmel_mxt_ts 2-004a: Interrupt triggered but zero messages",so,android can't work.

so,where is the problem?can anybody give any ideas?

0 项奖励
回复

4,772 次查看
aravinthkumarja
Senior Contributor II

Hi taowang1​,

Can you try following bootargs,

bootcmd=booti mmc1

loadaddr=0x80800000

stdout=serial

stdin=serial

stderr=serial

Regards,

Aravinth

0 项奖励
回复

4,772 次查看
taowang1
Contributor I

Hi,aravinthkumar jayaprakasam

Thank you for your reply and suggestions.

The following is the result :

=> setenv bootcmd 'booti mmc1'

=> setenv loadaddr 0x80800000

=> setenv stdout serial

=> setenv stdin serial

=> setenv stderr serial

=> pri

baudrate=115200

bootcmd=booti mmc1

bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

bootcmd_mmc=mmc dev ${mmcdev}; mmc read ${loadaddr} 0x800 0x3800; booti ${loadaddr}

bootdelay=0

fastboot_dev=mmc1

fdt_high=0xffffffff

initrd_addr=0x12C00000

initrd_high=0xffffffff

loadaddr=0x80800000

mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off

mmcdev=1

splashpos=m,m

stderr=serial

stdin=serial

stdout=serial

Environment size: 642/8188 bytes

=> boot

booti mmc1

can't find partition: boot, dump the partition table

ptn 0  name=bootloader_nor  start=0        len=393216   0x00000000~0x00060000

ptn 1  name=kernel_nor      start=393216   len=3145728  0x00060000~0x00360000

ptn 2  name=dtb_nor         start=3538944  len=262144   0x00360000~0x003A0000

ptn 3  name=recovery_nor    start=3801088  len=4194304  0x003A0000~0x007A0000

ptn 4  name=burn_nor        start=0        len=8388608  0x00000000~0x00800000

ptn 5  name=mbr             start=0        len=1        0x000000000~0x000000200

ptn 6  name=bootloader      start=2        len=2046     0x000000400~0x000100000

ptn 7  name=bootimg         start=2048     len=14336    0x000100000~0x000800000

ptn 8  name=boottestsuit    start=16384    len=6144     0x000800000~0x000B00000

ptn 9  name=bootparams      start=22528    len=2048     0x000B00000~0x000C00000

ptn 10 name=bootreserved    start=24576    len=8192     0x000C00000~0x001000000

ptn 11 name=recovery        start=32768    len=32768    0x001000000~0x002000000

ptn 12 name=sdcard          start=65536    len=18874368 0x002000000~0x242000000

ptn 13 name=system          start=18939905 len=2097151  0x242000200~0x282000000

ptn 14 name=data            start=21037057 len=2097151  0x282000200~0x2C2000000

ptn 15 name=cache           start=23134209 len=262143   0x2C2000200~0x2CA000000

ptn 16 name=private         start=23396353 len=4194303  0x2CA000200~0x34A000000

ptn 17 name=keyinfo         start=27590657 len=32767    0x34A000200~0x34B000000

ptn 18 name=reserved        start=27623425 len=131071   0x34B000200~0x34F000000

ptn 19 name=map             start=27754497 len=33316863 0x34F000200~0x747C00000

booti: cannot find 'boot' partition

fastboot is in init......

ptn 0  name=bootloader_nor  start=0        len=393216   0x00000000~0x00060000

ptn 1  name=kernel_nor      start=393216   len=3145728  0x00060000~0x00360000

ptn 2  name=dtb_nor         start=3538944  len=262144   0x00360000~0x003A0000

ptn 3  name=recovery_nor    start=3801088  len=4194304  0x003A0000~0x007A0000

ptn 4  name=burn_nor        start=0        len=8388608  0x00000000~0x00800000

ptn 5  name=mbr             start=0        len=1        0x000000000~0x000000200

ptn 6  name=bootloader      start=2        len=2046     0x000000400~0x000100000

ptn 7  name=bootimg         start=2048     len=14336    0x000100000~0x000800000

ptn 8  name=boottestsuit    start=16384    len=6144     0x000800000~0x000B00000

ptn 9  name=bootparams      start=22528    len=2048     0x000B00000~0x000C00000

ptn 10 name=bootreserved    start=24576    len=8192     0x000C00000~0x001000000

ptn 11 name=recovery        start=32768    len=32768    0x001000000~0x002000000

ptn 12 name=sdcard          start=65536    len=18874368 0x002000000~0x242000000

ptn 13 name=system          start=18939905 len=2097151  0x242000200~0x282000000

ptn 14 name=data            start=21037057 len=2097151  0x282000200~0x2C2000000

ptn 15 name=cache           start=23134209 len=262143   0x2C2000200~0x2CA000000

ptn 16 name=private         start=23396353 len=4194303  0x2CA000200~0x34A000000

ptn 17 name=keyinfo         start=27590657 len=32767    0x34A000200~0x34B000000

ptn 18 name=reserved        start=27623425 len=131071   0x34B000200~0x34F000000

ptn 19 name=map             start=27754497 len=33316863 0x34F000200~0x747C00000

USB Mini b cable Connected!

fastboot initialized

USB_SUSPEND

USB_RESET

USB_PORT_CHANGE 0x4

USB_SUSPEND

USB_RESET

USB_PORT_CHANGE 0x4

USB_SUSPEND

USB_RESET

USB_PORT_CHANGE 0x4

USB_SUSPEND

0 项奖励
回复

4,771 次查看
aravinthkumarja
Senior Contributor II

Hi taowang​,

Give below command and set the environment.

=> env default -f -a

=> env save

Then you give bootargs,

=> setenv bootcmd 'booti mmc1'

=> setenv loadaddr 0x80800000

=> setenv stdout serial

=> setenv stdin serial

=> setenv stderr serial

Regards,

Aravinth

0 项奖励
回复

4,771 次查看
taowang1
Contributor I

Hi,Aravinth

Thank you for youre quick reply!

I do it as your suggestion again,

The log is the same as above.

Any additonal suggestion?

0 项奖励
回复

4,771 次查看
aravinthkumarja
Senior Contributor II

Hi tao,

Remaining is only ddr stress test.

Regards,

Aravinth

0 项奖励
回复

4,771 次查看
taowang1
Contributor I

The additional information :

the uboot environment is as follows:

=> > pri

baudrate=115200

bootcmd=run bootcmd_mmc

bootcmd_mfg=run mfgtool_args;bootz ${loadaddr} ${initrd_addr} ${fdt_addr};

bootcmd_mmc=mmc dev ${mmcdev}; mmc read ${loadaddr} 0x800 0x3800; booti ${loadaddr}

bootdelay=0

fastboot_dev=mmc1

fdt_high=0xffffffff

initrd_addr=0x12C00000

initrd_high=0xffffffff

loadaddr=0x12000000

mfgtool_args=setenv bootargs console=ttymxc0,115200 rdinit=/linuxrc g_mass_storage.stall=0 g_mass_storage.removable=1 g_mass_storage.idVendor=0x066F g_mass_storage.idProduct=0x37FF g_mass_storage.iSerialNumber="" enable_wait_mode=off

mmcdev=1

splashpos=m,m

Environment size: 600/8188 bytes

0 项奖励
回复

4,771 次查看
igorpadykov
NXP Employee
NXP Employee

also hanging may be caused by ddr errors, as for custom board

ddr test should be run and uboot updated with new calibration

coefficients.

https://community.freescale.com/docs/DOC-105652

Best regards

igor

0 项奖励
回复

4,771 次查看
taowang1
Contributor I

Hi,igorpadykov

I did the DDR calibration and DDR stress test ,both gain success.

0 项奖励
回复