imx6q - parallel RGB display support

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6q - parallel RGB display support

1,397 次查看
ashasampathkuma
Contributor I

Hi everyone ,

Our custom board is based on imx6q . We need to interface parallel RGB display to our custom board . We modified the below settings in dtsi file

mxcfb1: fb@0 {
        compatible = "fsl,mxc_sdc_fb";
        disp_dev = "lcd";
        interface_pix_fmt = "RGB24";                
        default_bpp = <24>;
        int_clk = <0>;
        late_init = <0>;
        status = "disabled";
        mode_str="LCD"       
    };

lcd@0 {

compatible = "fsl,lcd";

ipu_id= <0>

disp_id = <0>

default_ifmt="RGB24"

pinctrl_names="default"

pinctrl-0= <&pinctrl_ipu1>

status = "okay"

};

&ldb {
    status = "disabled";

    lvds-channel@0 {
        fsl,data-mapping = "spwg";
        fsl,data-width = <24>;
        primary;
        status = "disabled";

        display-timings {
            native-mode = <&timing0>;
            timing0: hsd100pxn1 {
                clock-frequency = <51000000>;
                hactive = <1024>;
                vactive = <600>;
                hback-porch = <160>;
                hfront-porch = <80>;
                vback-porch = <19>;
                vfront-porch = <8>;
                hsync-len = <60>;
                vsync-len = <8>;
            };
        };
    };

    lvds-channel@1 {
        fsl,data-mapping = "spwg";
        fsl,data-width = <18>;
        status = "disabled";

        display-timings {
            native-mode = <&timing1>;
            timing1: hsd100pxn1 {
                clock-frequency = <65000000>;
                hactive = <1024>;
                vactive = <768>;
                hback-porch = <220>;
                hfront-porch = <40>;
                vback-porch = <21>;
                vfront-porch = <7>;
                hsync-len = <60>;
                vsync-len = <10>;
            };
        };
    };
};

then video/fbdev/mxc/mxc_lcdif.c added

static struct fb_videomode lcdif_modedb[] = {
    {
    /*custom display */
    "LCD", 60, 720, 1280,12987, 72, 56, 38, 3, 128, 10,     // from custom LCD datasheet
    FB_SYNC_CLK_LAT_FALL,                                      //
    FB_VMODE_NONINTERLACED,
    0,}, 
};

Problem is there is no pixel clock generated (checked by probing disp0_clk line).

But in cat  /sys/kernel/debug/clk/ipu1_pclk0/clk_rate displays 77 MHZ

Is there any other setting missed ? Kindly help me in resolving this issue.

Thanks

Asha

0 项奖励
回复
1 回复

1,190 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Asha

for i.MX6Q parallel RGB display support may be useful to check

Configuring i.MX6 boards for different screens - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复