imx6dl boot source

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6dl boot source

1,676件の閲覧回数
arkadiuszkaras
Contributor I

Hello,

With imx6, is there any possibility to check from which interface ROM loaded boot stream ?

I need to know in u-boot from which device it was loaded.

Regards

AK

ラベル(7)
タグ(2)
0 件の賞賛
返信
1 返信

1,557件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Arkadiusz

yes, this could be done using

SRC Boot Mode Register 1 (SRC_SBMR1,2)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信