imx6dl boot source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6dl boot source

1,683 Views
arkadiuszkaras
Contributor I

Hello,

With imx6, is there any possibility to check from which interface ROM loaded boot stream ?

I need to know in u-boot from which device it was loaded.

Regards

AK

Tags (2)
0 Kudos
Reply
1 Reply

1,564 Views
igorpadykov
NXP Employee
NXP Employee

Hi Arkadiusz

yes, this could be done using

SRC Boot Mode Register 1 (SRC_SBMR1,2)

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply