i.MX6SDL V4L2 driver issue.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6SDL V4L2 driver issue.

1,482 Views
satoshishimoda
Senior Contributor I

Hi community,

I have a problem about i.MX6SDL V4L2 driver.

When execute the following procedure, output image is strange on process 8.

(A image which should be located to the left part is displayed to right part)

[Procedure]

1. Open driver.

2. Execute *Setting 1.

3. Output image (VIDIOC_STREAMON)

4. Stop output image (VIDIOC_STREAMOFF)

5. Close driver.

6. Open driver.

7. Execute *Setting 2.

8. Output image (VIDIOC_STREAMON)

Then, if change *Setting 1 to *Setting 3, this issue was not occurred.

=====

*Setting 1:

[VIDIOC_S_CROP]

top=24

left=0

width=1024

height=720

[VIDIOC_S_FMT]

fmt.fmt.pix.width=1280

fmt.fmt.pix.height=720

v4l2_rect(4l2_format::fmt.pix.priv)

 .top=0,.left=128,.width=1024, height=720

fmt.type = V4L2_BUF_TYPE_VIDEO_OUTPUT

fmt.fmt.pix.pixelformat=V4L2_PIX_FMT_NV12

*Setting 2:

[VIDIOC_S_CROP]

top=24

left=0

width=1024

height=720

[VIDIOC_S_FMT]

fmt.fmt.pix.width=1280

fmt.fmt.pix.height=720

v4l2_rect(4l2_format::fmt.pix.priv)

 .top=0,.left=0,.width=1024, height=720

fmt.type = V4L2_BUF_TYPE_VIDEO_OUTPUT

fmt.fmt.pix.pixelformat=V4L2_PIX_FMT_NV12

*Setting 3:

[VIDIOC_S_CROP]

top=24

left=0

width=1024

height=720

[VIDIOC_S_FMT]

fmt.fmt.pix.width=1280

fmt.fmt.pix.height=720

v4l2_rect(4l2_format::fmt.pix.priv)

 .top=0,.left=32,.width=960, height=720

fmt.type = V4L2_BUF_TYPE_VIDEO_OUTPUT

fmt.fmt.pix.pixelformat=V4L2_PIX_FMT_NV12

=====

We investigated the root cause and found a solution, but not resolved completely.

=====

[Root Cause]

In show_buf() function (line 535) in drivers/media/video/mxc/output/mxc_vout.c, "var.xoffset" is not updated to "0" when not set "bypass".

And if update "var.xoffset" when set "bypass", it cannot return the value when not set "bypass".

[Solution]

Add "var.xoffset = 0" on back line 562.

[Remained Issue]

Change the output image form set "bypass" to not set "bypass", the image is output with the var.xoffset value which is the one when set "bypass" about 1 frame.

So the issue I said at first is occurred momentary.

=====

Would you give me a advice to resolve this issue completely?

The above procedure or solution was wrong?

Best Regards,

Satoshi Shimoda

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,239 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Satoshi Shimoda,

Do you still have this issue? Would you please provide the source code which can execute your procedures so we can replicate it?

Regards,

0 Kudos
Reply