imx6dl SPI timing issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6dl SPI timing issue

2,693 次查看
Anonymous
不适用

Dear all,

I'm using following kind of Kernel ver. with i.MX6DL.

https://github.com/Freescale/linux-fslc/tree/4.14-1.0.x-imx

I'm facing SPI communication problem.

At the first packet of SPI communication,  SPI_CLK become High↑  after CS becomes Low ↓.
That's why the MSB bit always becomes "1". 

Send data "14 00 00 10 FF" -> 0b1 + 0x14 + 0x00 + ... -> Receive data "8A 00 00 08 7F"

SPI1_CS1.png

With another CS device , we can see same phenomenon for the first packet.

Send data "00 00 xx" -> 0b1 + 0x00 + 0x00 -> Receive data "80 00 xx"

SPI1_CS3.png

For the same device, there is no problem from 2nd packet as long as I checked.

But I don't know the root cause of this phenomenon, and when this problem happen.

In my environment, there is no EVK board, so this problem can be seen only with my own board with SPI1_cs1, cs2, cs3, SPI2_cs2.

Is there any way to avoid this problem?

Best regards,

标签 (1)
0 项奖励
回复
8 回复数

2,415 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nanao

may be recommended to test with official nxp kernels from

source.codeaurora.org/external/imx/linux-imx  repository:

linux-imx - i.MX Linux kernel 

Linux 5.4.3_1.0.0 Documentation

mxc_spi_test\test - imx-test - i.MX Driver Test Application Software 

"linux-fslc" kernels are supported by community and issue may be posted

on meta-fsl-arm mailing list

meta-freescale@lists.yoctoproject.org | Home 

Differencies between kernels are described on

difference between Yocto Community BSP and Freescale BSP Release 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,415 次查看
Anonymous
不适用

Hi igorpadykov,

Thank you for your comment.

I checked the Kernel ver. again, and found that the correct ver. is following one.

https://source.codeaurora.org/external/imx/linux-imx/?h=imx_4.14.98_2.0.0_ga

Could you please give me any other advice?

Best reagrds,
Nanao.

0 项奖励
回复

2,415 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nanao

also one can test with baremetal sdk test (folder ../drivers/spi), then compare

ecspi settings with linux. "1.1.0_iMX6_Platform_SDK.zip"

on link SMP Enable in IMX6 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,415 次查看
Anonymous
不适用

Hi igorpadykov,

Thank you for your reply.

Now it's difficult to test with baremetal sdk test with my environment.

By the way, I found the another thread and it looks like similar problem.

i.MX6 ecspi race condition with CPOL=1 and CS GPIO 

Our Ver. is later than "imx_4.14.78_1.0.0_ga release".

Do you know there is any other patch?

Best regards,

Nanao.

0 项奖励
回复

2,415 次查看
Anonymous
不适用

Hi igorpadykov,

We found that this issue happen with SPI Mode3.

Default_MS21r5.png

If I changed the setting from Mode3 to Mode0, CLK and data are no problem.

mode3⇒0.png

And I tried adding 50us delay as Théo mentioned at i.MX6 ecspi race condition with CPOL=1 and CS GPIO 

/* CTRL register always go first to bring out controller from reset */
writel(ctrl, spi_imx->base + MX51_ECSPI_CTRL);

udelay(50);

reg = readl(spi_imx->base + MX51_ECSPI_TESTREG);
if (spi->mode & SPI_LOOP)
reg |= MX51_ECSPI_TESTREG_LBC;
else
reg &= ~MX51_ECSPI_TESTREG_LBC;
writel(reg, spi_imx->base + MX51_ECSPI_TESTREG);

writel(cfg, spi_imx->base + MX51_ECSPI_CONFIG);

But it does not have good effect for my case.  (Our speed is 3MHz.)

udelya50.png

This slave device can used only with SPI Mode 3, so I cannot change Mode.

At least we would like to know if this issue happen only for the first packet or not.

If someone knows that this is a known issue, please let us know.

Best regards,

Nanao Akimichi.

0 项奖励
回复

2,415 次查看
igorpadykov
NXP Employee
NXP Employee

HI Nanao

one can try with Sabre-AI image imx6dl-sabreauto-ecspi.dts :

imx6dl-sabreauto-ecspi.dts\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

try to work without dma (remove dma entries in ecspi1: ecspi@02008000 {..)

imx6qdl.dtsi\dts\boot\arm\arch - linux-imx - i.MX Linux kernel 

Best regards
igor

0 项奖励
回复

2,415 次查看
Anonymous
不适用

Hi igor,

Without dma doesn't work, however, we can see that the wrong timing issue disappear by adding following 3 lines.

u32 sclk_val = 15;

writel(MX51_ECSPI_CTRL_ENABLE | MX51_ECSPI_CTRL_MODE_MASK, spi_imx->base + MX51_ECSPI_CTRL);

writel(sclk_val << 20 | sclk_val << 4, spi_imx->base + MX51_ECSPI_CONFIG);

This will be  a temporary solution for us.

If there is another official solution, let us know.

Thank you for your help.

Best Regards,

Nanao Akimichi.

0 项奖励
回复

2,415 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Nanao

I will check internally and send details via mail.

Best regards
igor

0 项奖励
回复