(imx6) reference design for bluetooth HFP/HSP ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

(imx6) reference design for bluetooth HFP/HSP ?

Jump to solution
3,195 Views
cxh
Fresh Out Contributor

Hi,

Is there a reference design for bluetooth HFP/HSP?

Now we get A2DP work on iMX6 with sgtl5000 and rtl8723,

but failed to implement HFP/HSP.

Best Regards,

xh

Labels (1)
0 Kudos
Reply
1 Solution
2,767 Views
igorpadykov
NXP Employee
NXP Employee

Hi xh

I am afraid there is no such design, please refer to p.4 attached release

notes for supported profiles in last L5.0.0_1.0.0 android release.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
2,768 Views
igorpadykov
NXP Employee
NXP Employee

Hi xh

I am afraid there is no such design, please refer to p.4 attached release

notes for supported profiles in last L5.0.0_1.0.0 android release.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply