Freescale processor with safety standards

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freescale processor with safety standards

1,523 Views
sumeetdube
Contributor III

Hi all,

I wanted to know if any Freescale processor supports following safety and industrial standards

1. Safety level sil4

2. Industry standard IEC61508

3. Automotive standard ISO26262

We would like to use IMX . Does iMX6q support above standards or could it be certified?

Thank you.

Labels (1)
0 Kudos
Reply
1 Reply

1,443 Views
b36401
NXP Employee
NXP Employee

No. i.MX6q was not certified for these standards.

Sorry for the inconvenience.

Have a great day,

Victor

-----------------------------------------------------------------------------------------------------------------------                                                            

Note: If this post answers your question, please click the Correct Answer button. Thank you!                                                                                       

-----------------------------------------------------------------------------------------------------------------------                                                            

0 Kudos
Reply