imx6 SoloX; USB error attempting to run DDR Test Tool V2.51

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 SoloX; USB error attempting to run DDR Test Tool V2.51

2,202 Views
bap3ball
Contributor III

Does the DDR Test Tool v2.51 support the SoloX Sabre Eval board?

Tried running this tool on both my custom hardware and the Sabre board (via USB OTG) and both give the following error message. There are no files in the tools log folder.

pastedImage_0.png

Labels (2)
0 Kudos
Reply
3 Replies

1,923 Views
Yuri
NXP Employee
NXP Employee

Hello,

  Please try the enclosed previous release.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,923 Views
bap3ball
Contributor III

Thanks.

The 2.50 version appears to run properly.

Unfortunately fails calibration on our hardware.

0 Kudos
Reply

1,923 Views
BiyongSUN
NXP Employee
NXP Employee

Please submit your issue to the following ticket. The DDR stress test owner is supporting the following ticket.

i.MX6/7 DDR Stress Test Tool V2.51