imx6 SoloX; USB error attempting to run DDR Test Tool V2.51

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 SoloX; USB error attempting to run DDR Test Tool V2.51

2,453件の閲覧回数
bap3ball
Contributor III

Does the DDR Test Tool v2.51 support the SoloX Sabre Eval board?

Tried running this tool on both my custom hardware and the Sabre board (via USB OTG) and both give the following error message. There are no files in the tools log folder.

pastedImage_0.png

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

2,174件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Please try the enclosed previous release.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,174件の閲覧回数
bap3ball
Contributor III

Thanks.

The 2.50 version appears to run properly.

Unfortunately fails calibration on our hardware.

0 件の賞賛
返信

2,174件の閲覧回数
BiyongSUN
NXP Employee
NXP Employee

Please submit your issue to the following ticket. The DDR stress test owner is supporting the following ticket.

i.MX6/7 DDR Stress Test Tool V2.51