imx6 MIPI input 60fps

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 MIPI input 60fps

ソリューションへジャンプ
2,270件の閲覧回数
zhencongtee
Contributor III

Hi,

May I know does the i.mx6 Solo support camera MIPI input up to 60fps at 1024x768 resolution?

Thank you.

Regards,

Zhen Cong Tee

ラベル(4)
タグ(3)
0 件の賞賛
返信
1 解決策
1,847件の閲覧回数
Yuri
NXP Employee
NXP Employee

MIPI CSI-2 supports from 80 Mbps to 800 Mbps speed per data lane.

The CSI-2 Receiver core can manage one clock lane and up to two data lanes.

Each i.MX 6Solo/6DualLite processor has two lanes.

 
Basically it is enough to support 60fps at 1024x768.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,848件の閲覧回数
Yuri
NXP Employee
NXP Employee

MIPI CSI-2 supports from 80 Mbps to 800 Mbps speed per data lane.

The CSI-2 Receiver core can manage one clock lane and up to two data lanes.

Each i.MX 6Solo/6DualLite processor has two lanes.

 
Basically it is enough to support 60fps at 1024x768.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信