imx6 MIPI input 60fps

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 MIPI input 60fps

Jump to solution
2,266 Views
zhencongtee
Contributor III

Hi,

May I know does the i.mx6 Solo support camera MIPI input up to 60fps at 1024x768 resolution?

Thank you.

Regards,

Zhen Cong Tee

Tags (3)
0 Kudos
Reply
1 Solution
1,843 Views
Yuri
NXP Employee
NXP Employee

MIPI CSI-2 supports from 80 Mbps to 800 Mbps speed per data lane.

The CSI-2 Receiver core can manage one clock lane and up to two data lanes.

Each i.MX 6Solo/6DualLite processor has two lanes.

 
Basically it is enough to support 60fps at 1024x768.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,844 Views
Yuri
NXP Employee
NXP Employee

MIPI CSI-2 supports from 80 Mbps to 800 Mbps speed per data lane.

The CSI-2 Receiver core can manage one clock lane and up to two data lanes.

Each i.MX 6Solo/6DualLite processor has two lanes.

 
Basically it is enough to support 60fps at 1024x768.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply