imx6 LCD 20 bit YUV option in Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx6 LCD 20 bit YUV option in Linux

1,287件の閲覧回数
abeeshmp_dct
Contributor II

Hi Team, 

 

I have a requirement to connect the imx6q to a display device which accept 20 bit YUV video. As I checked in datasheet , I could see the option is available as shown below, 

20bit option.png

But  I didn't see any option to enable this in the TRM as well as in the latest Linux kernel available. 

 

Could you please comment on the availability of this feature in the latest Kernel? or Any patch available for this?

 

0 件の賞賛
返信
2 返答(返信)

1,278件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ABEESH

 

one can look at patches provided on

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-Support-BT656-and-BT1120-Output...

 

Best regards
igor

0 件の賞賛
返信

1,274件の閲覧回数
abeeshmp_dct
Contributor II

Hi Igor,

 

Thanks for the reply.

That patches has suppprt for 16 bit yuv, but not 20bit YUV. What we need is 20bit yuv output with external sync signals.

Can you please help on that.

0 件の賞賛
返信