imx6 LCD 20 bit YUV option in Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6 LCD 20 bit YUV option in Linux

1,288 Views
abeeshmp_dct
Contributor II

Hi Team, 

 

I have a requirement to connect the imx6q to a display device which accept 20 bit YUV video. As I checked in datasheet , I could see the option is available as shown below, 

20bit option.png

But  I didn't see any option to enable this in the TRM as well as in the latest Linux kernel available. 

 

Could you please comment on the availability of this feature in the latest Kernel? or Any patch available for this?

 

0 Kudos
Reply
2 Replies

1,279 Views
igorpadykov
NXP Employee
NXP Employee

Hi ABEESH

 

one can look at patches provided on

https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Patch-to-Support-BT656-and-BT1120-Output...

 

Best regards
igor

0 Kudos
Reply

1,275 Views
abeeshmp_dct
Contributor II

Hi Igor,

 

Thanks for the reply.

That patches has suppprt for 16 bit yuv, but not 20bit YUV. What we need is 20bit yuv output with external sync signals.

Can you please help on that.

0 Kudos
Reply