MC33PF100 Reset Pin Wiring for IMXQM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MC33PF100 Reset Pin Wiring for IMXQM

523 Views
CircuitPeon
Contributor I

Hello,

 

I am designing with an IMX8QM and see that it is recommended to use both MC33PF8100EPES and MC33PF8100EQES. This is correct?

 

Would it be recommended to directly connect both PMIC 'RESET_MCU' directly to the IMX8 POR_B? 

 

Thank you!

0 Kudos
Reply
1 Reply

515 Views
igorpadykov
NXP Employee
NXP Employee

Hi Brandon

 

>it is recommended to use both MC33PF8100EPES and MC33PF8100EQES. This is correct?

 

yes as described in Table 2. Ordering information   PF8100_PF8200, 12-channel power management integrated circuit for high performance applications - Da...

 

>Would it be recommended to directly connect both PMIC 'RESET_MCU' directly to the IMX8 POR_B?

 

yes, one can look at  MCIMX8QM-CPU MEK – Schematics

 

Best regards
igor

 

0 Kudos
Reply