imx287 boot failure

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx287 boot failure

3,080 次查看
adityapatil
Contributor II

hi ,

1. I have a custom board designed with imx287 CPU

2. The NAND flash is MT29F1G08ABBDAHC-IT:D and RAM is MT47H128M16RT-25E.

I am getting the following Problems

1. If try to reset from " uboot > reset"  or do a power-up.

most of  the time board fails and i get the following LOG

 

MX28 U-Boot > reset
resetting ...

PowerPrep start initialize power...

Configured for 5v only power source. Battery powered operation disabled.

PowerPrep start initialize power...

Configured for 5v only power source. Battery powered operation disabled.

PowerPrep start initialize power...

Configured for 5v only power source. Battery powered operation disabled.

PowerPrep start initialize power...

Configured for 5v only power source. Battery powered operation disabled.

Thanks

-aditya

标签 (2)
标记 (1)
0 项奖励
回复
3 回复数

2,665 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Aditya

what about cold boot (not uboot reset), is it booting fine.

5v only power source mode is added with L2.6.35_1.1.0_130130 patch

Compile L2.6.35_1.1.0_130130 for i.MX28 on Ubuntu 13.10 64bit OS 

For new ddr support please look on

https://community.nxp.com/docs/DOC-1455 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,665 次查看
adityapatil
Contributor II

hi,

The cold boot is fine only for most of my custom boards but some custom boards I always get same boot failure output.

Thanks,

-aditya

0 项奖励
回复

2,665 次查看
igorpadykov
NXP Employee
NXP Employee

for uboot reset issue please post this on uboot mail list

U-Boot Info Page 

for cold boot issue one can test memory (mem_test.7z.zip)

i.MX28 DDR stress test 

Best regards
igor

0 项奖励
回复