imx28 fresh board usb boot from linux host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx28 fresh board usb boot from linux host

1,648 Views
bibinb
Contributor I

i have a fresh custom board with imx28 with USB as the only first time boot option. Is there any tool to boot imx28 from linux host PC(preferably ubuntu).

Labels (2)
0 Kudos
Reply
3 Replies

1,364 Views
fabio_estevam
NXP Employee
NXP Employee

You can use mxsldr:

3.1.5 USB Firmware Upload | www.denx-cs.de/doku

Regards,

Fabio Estevam

0 Kudos
Reply

1,364 Views
igorpadykov
NXP Employee
NXP Employee

Hi bibin

one can try mfg tool for programming fresh board with usb

Programmers (Flash, etc.) (8)

Tool and documentation for downloading i.MX28 image during manufacturing (REV L2.6.35_1.1.0)

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,364 Views
bibinb
Contributor I

Thanks igor for the reply.

This tool will work only in Windows OS. Right?

Is there any tool available for ubuntu or other linux distros?

0 Kudos
Reply