imx28 fresh board usb boot from linux host

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 fresh board usb boot from linux host

1,685件の閲覧回数
bibinb
Contributor I

i have a fresh custom board with imx28 with USB as the only first time boot option. Is there any tool to boot imx28 from linux host PC(preferably ubuntu).

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

1,401件の閲覧回数
fabio_estevam
NXP Employee
NXP Employee

You can use mxsldr:

3.1.5 USB Firmware Upload | www.denx-cs.de/doku

Regards,

Fabio Estevam

0 件の賞賛
返信

1,401件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi bibin

one can try mfg tool for programming fresh board with usb

Programmers (Flash, etc.) (8)

Tool and documentation for downloading i.MX28 image during manufacturing (REV L2.6.35_1.1.0)

http://www.freescale.com/products/arm-processors/i.mx-applications-processors-based-on-arm-cores/i.m...

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,401件の閲覧回数
bibinb
Contributor I

Thanks igor for the reply.

This tool will work only in Windows OS. Right?

Is there any tool available for ubuntu or other linux distros?

0 件の賞賛
返信