i.Mx6 Quad support for Wifi interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

i.Mx6 Quad support for Wifi interface

1,723件の閲覧回数
nanjundam
Contributor II

Hi,

I'm using the i.Mx6 Quad processor in my design. It has 4 SD Interfaces (SD1, SD2, SD3, SD4).

In these SD1 and SD2 are 4 bit SDIO interfaces and SD3 and SD4 are 8 bit interfaces.

In My design, I've used the SD2, SD3, SD4 for other interfaces and SD1 I'm using for Wifi interface.

I'm designing the Wifi for 802.11b/g/n speed standards.

Can you please tell me, will this speed and interface are supported by the device(i.Mx6x -MCIMX6Q6AVT10)

Please reply ASAP.

Thanks for the reply in advance.

Regards,

Nanjunda M

ラベル(3)
タグ(3)
0 件の賞賛
返信
2 返答(返信)

1,460件の閲覧回数
nanjundam
Contributor II

Thanks for the response.

Regards,

Nanjunda M

0 件の賞賛
返信

1,460件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Nanjunda

supported max. speed for SD and SDIO cards up to

104MB/s (UHS-I SDR104 mode), so seems these standards can

be supported.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信