imx28 error!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

imx28 error!

1,849件の閲覧回数
chengyouping
Contributor I

download updated imx28 bsp.

ltib and execution in imx28 dvk,

result is as following.

root@freescale ~/mp3$ root@freescale ~/mp3gst-launch filesrc location=test.wav !

wavparse ! mfw_mp3encoder ! filesink location=output.mp3

-sh: root@freescale: not found

root@freescale ~/mp3$ gst-launch alsasrc num-buffers=240 blocksize=44100 ! mfw_m

p3encoder ! filesink location=output.mp3

BLN_MAD-MMCODECS_MP3E_ARM_02.02.00_ARM9  build on Mar 21 2012 17:11:54.

MFW_GST_MP3_ENCODER_PLUGIN 3.0.6 build on Feb 13 2014 08:33:57.

Setting pipeline to PAUSED ...

sgtl5000_write: write reg error : Reg 0x06 = 0x0000

sgtl5000_write: write reg error : Reg 0x04 = 0x0000

sgtl5000_write: write reg error : Reg 0x06 = 0x0130

sgtl5000_write: write reg error : Reg 0x02 = 0x0002

sgtl5000_write: write reg error : Reg 0x30 = 0x5a62

sgtl5000_write: write reg error : Reg 0x30 = 0x5a7b

sgtl5000_write: write reg error : Reg 0x02 = 0x0022

sgtl5000_write: write reg error : Reg 0x02 = 0x0062

sgtl5000_write: write reg error : Reg 0x2a = 0x0200

sgtl5000_write: write reg error : Reg 0x30 = 0x5afb

sgtl5000_hw_read: read reg error : Reg 0x0e

sgtl5000_write: write reg error : Reg 0x0e = 0x0000

Pipeline is live and does not need PREROLL ...

Setting pipeline to PLAYING ...

New clock: GstAudioSrcClock

Caught interrupt -- handling interrupt.

Interrupt: Stopping pipeline ...

Execution ended after 37207937317 ns.

Setting pipeline to PAUSED ...

Setting pipeline to READY ...

sgtl5000_write: write reg error : Reg 0x30 = 0x5ab9

sgtl5000_write: write reg error : Reg 0x02 = 0x0060

sgtl5000_write: write reg error : Reg 0x06 = 0x0130

sgtl5000_write: write reg error : Reg 0x2a = 0x0000

sgtl5000_write: write reg error : Reg 0x30 = 0x5a39

sgtl5000_write: write reg error : Reg 0x02 = 0x0060

sgtl5000_write: write reg error : Reg 0x02 = 0x0020

sgtl5000_hw_read: read reg error : Reg 0x0e

sgtl5000_write: write reg error : Reg 0x0e = 0x000c

sgtl5000_write: write reg error : Reg 0x30 = 0x5a20

sgtl5000_write: write reg error : Reg 0x02 = 0x0000

root@freescale ~/mp3$ gst-launch filesrc location=output.mp3 typefind=true ! bee

pdec ! audioconvert ! 'audio/x-raw-int, channels=2' ! alsasink

Setting pipeline to PAUSED ...

sgtl5000_write: write reg error : Reg 0x06 = 0x0000

sgtl5000_write: write reg error : Reg 0x04 = 0x0000

sgtl5000_write: write reg error : Reg 0x06 = 0x0130

sgtl5000_write: write reg error : Reg 0x02 = 0x0001

sgtl5000_write: write reg error : Reg 0x30 = 0x5a39

sgtl5000_write: write reg error : Reg 0x02 = 0x0021

sgtl5000_write: write reg error : Reg 0x24 = 0x0022

sgtl5000_write: write reg error : Reg 0x2a = 0x0200

sgtl5000_write: write reg error : Reg 0x30 = 0x5ab9

sgtl5000_hw_read: read reg error : Reg 0x0e

sgtl5000_write: write reg error : Reg 0x0e = 0x0000

ERROR: Pipeline doesn't want to pause.

ERROR: from element /GstPipeline:pipeline0/GstFileSrc:filesrc0: Could not determ

ine type of stream.

Additional debug info:

gstbasesrc.c(2795): gst_base_src_start (): /GstPipeline:pipeline0/GstFileSrc:fil

esrc0

Setting pipeline to NULL ...

sgtl5000_hw_read: read reg error : Reg 0x0e

sgtl5000_write: write reg error : Reg 0x0e = 0x000c

sgtl5000_write: write reg error : Reg 0x02 = 0x0020

sgtl5000_write: write reg error : Reg 0x06 = 0x0130

Freeing pipeline ...

root@freescale ~/mp3$ sgtl5000_write: write reg error : Reg 0x2a = 0x0000

sgtl5000_write: write reg error : Reg 0x30 = 0x5a39

sgtl5000_write: write reg error : Reg 0x02 = 0x0020

sgtl5000_write: write reg error : Reg 0x24 = 0x0132

sgtl5000_hw_read: read reg error : Reg 0x0e

sgtl5000_write: write reg error : Reg 0x0e = 0x000c

sgtl5000_write: write reg error : Reg 0x30 = 0x5a20

sgtl5000_write: write reg error : Reg 0x02 = 0x0000

root@freescale ~/mp3$ ls -l

-rw-r--r--    1 root     root             0 Jan  1 00:55 output.mp3

root@freescale ~/mp3$


why?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

1,555件の閲覧回数
Alvin
NXP Employee
NXP Employee

Hi youping.

Before using gstreamer, pls confirm that you have built and installed the FSL multimedia core libraries and gstreamer plugins. :smileyhappy:

0 件の賞賛
返信